We use bq256703A to route USB type C power to our system and charging a 3-cell battery. The setup works well in general. However, we observed that bq25703A could intermittently stop charging battery. The issue have been observed with multiple system and batteries. The fail scenario are very similar.
The charging starts at 10V battery voltage. With a volt meter, we can see that the battery voltage increasing to about 10.6V. The voltage gradually dropped to about 10.2V and stayed there. Our system can read the bq25703A internal registers. The charge status register at 0x20/21 has value of 0xa000. the bq25703A registers also show that VBus is 19.2V. Vsys is 10.432V, and Vbat is 10.240V. Those values are the same in all our tests (different boards and battery) showing the failure. Given the value of the charging status, we are not able to tell which charging mode bq25703A is in. Also, the battery changing complete correctly for most of our charging/discharging test. Although the occurrence of the failure is intermittent, the signature of the failure is consistent.
Did someone report similar issue in the past? Would additional information do you need?
Thanks,
Zhaohong