Other Parts Discussed in Thread: UCC24612, UCC24624
Is there an available drawing for HPA410A ?
It looks like the daughter card has a VDD ref... where does it come from ?
Thanks,
Ralph
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there an available drawing for HPA410A ?
It looks like the daughter card has a VDD ref... where does it come from ?
Thanks,
Ralph
Ralph
Figure 26 (page 17) of the UCC25600EVM User Guide https://www.ti.com/lit/ug/sluu361a/sluu361a.pdf is the schematic and Figure 24 and Figure 25 (page 16) are the copper layers for HPA410 daughter card.
You can refer to the pin designators on Figure 1 (page 4) schematic to determine how the various pins are connected. Please note that UCC25600EVM comes default populated with diode rectifier, so the logic VDD, GND and SYNC pins are not needed. If the HPA410 daughter cards are replaced with an SR controller like UCC24624 or UCC24612 then these logic pins would be used.
Best Regards,
Eric