This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27531-G1: the learning cycle does not start because update status is not set

Part Number: BQ27531-G1
Other Parts Discussed in Thread: BQSTUDIO

Hello,

I try to do a learning cycle with the bq27531 on my own board. Therefore I use the bqStudio withe the BQ27GDK000EVM and conected both with my board. I used the application note SLUA903 and carried out all the steps described. But after starting the leraning cycle (sending IT Enable and Reset), the update status did not change. It remains still 0x00. Nevertheless, I started to discharge and charge the battery. Still no change in update status.

When charging, I also noticed that FC is not set. To verify this I started another charging cycle (Stopcondition: FC is set). The bit was also not set during the test. Taper current was reached and the Voltage was higher than charging voltage minus taper voltage. However, I do not know whether the capacity requirement has been met. There are two different explanations in SLUUA96A.

Chapter 6.6.1.:

"accumulated change in capacity>Min TaperCharge"

Chapter 6.10.1.2.2.:

"Accumulated change in capacity<Min TaperCapacity"

Maybe both problems / observations have the same cause. Do you know of any similar problems, can you help me, or do you have a suggestion to try or investigate?

Thanks,

Steve