Other Parts Discussed in Thread: BQ34Z100-G1
Hello,
We have recently decided to increase the battery pack size of one of our products, using 21700 cells. The new design capacity should be 19600 mAh. I am not able to get Gauge Studio to accept a capacity above 15400 mAh. I notice that when the datasheet was revised to B, one of the changes was to reduce the capacity to 14500 mAh. However, 32Ah still appears widely in the datasheet and indeed on the product page of TI's web site. So I'm not clear if this is a bug in Gauge Studio, or am I hitting a poorly documented limit of the part.
Any advice would be greatly appreciated.
Just out of curiosity, if I were to set the design capacity to 15400, how would that affect the behavior of the gauging? Would it even pass a learn cycle?
Thanks, Ross