This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5121: recommended boost

Part Number: LM5121
Other Parts Discussed in Thread: LM5122

Hello team,

for a new project I'm looking for a boost powered by a battery, specs are Vin=14V, Vout=24V P=90W and I noticed the LM5121 and the 5122 without disconnection switch. Would there be a multi-phase controller (I would like to make my converter with 2 phases) that also manages synchronous rectification (therefore with integrated boostrap)?
Even one without synchronous rectification could work for me.
I would prefer to have a controller with integrated peak current mode.

Please let me know what your suggestions are.

Thanks and best regards,

Adrian

  • Hi Adrian,

    The 5122 is a synchronous controller and can implement dual-phase interleaved boost. It also utilizes peak current mode control. Please see section 8.1.3 of LM5122 datasheet for interleaved operation.

    This reference design (http://www.ti.com/tool/PMP9309) may be a starting point for your application. Keep in mind that you do not need to have the op-amp circuit as noted in the design.

    Thanks,

    Richard