Hi,
As I understand it, there are discrete current limit thresholds on the LM5166. The datasheet gives specific resistor values to connect to the ILIM pin to select one of them. What is the tolerance on those resistor values? If I wanted the 300mA out limit, for example, would I be okay using a 50k resistor? What would be the dangers of not using the exact values?
Ben