Other Parts Discussed in Thread: BQSTUDIO
Hello,
I have a standalone / removable battery pack with:
- the battery chemistry, Poly 3.7V one-cell 1000mAh
- a battery protection IC DW01-P from Chinese Fortune
- a battery charger LTC4067 from Linear
- a battery gauge BQ27542.
Without the TI battery gauge BQ27542, the current leak (the current measured at the pin + of the battery chemistry) is around 150 uA.
With the TI battery gauge BQ27542, the current leak is around 1750uA. So BQ27542 is using around 1.5mA which is a lot. It will drain the battery in one month. And it's what I'm seeing.
Is it normal to have such high current leak for BQ27542? Is there a way (software settings) to lower that amount?
PS: I can provide the schematics in a private message.