Other Parts Discussed in Thread: LP55231
I started with the LP55231 on my project but realized I needed a sinking driver instead, so I ended up at the LP5569. There are many similarities but the most notable exception is V1P8 on the LP5569.
The datasheet says it is the "Input power for digital circuitry" but with current draw under 200 µA and none of the digital inputs limited to a value relative to V1P8, is it really just a logic reference for the digital circuitry rather than an actual power supply?
To make a long story short, I'll power the LP5569 from a 5V rail and I'm considering using a super cheap 1.8V reference for the V1P8 pin rather than a regulator, and leaving the I2C lines pulled up to the MCU's 3.3V logic. Is there any issue with this approach?