Hi all
I am checking the possibility of using BQ78PL116 & BQ76PL102 with LiFePO4 8S1P pack.
1)as I understand BQ78PL116 has a gas gauge embedded and the software that we are using is BQwizard.
does BQwizard has a chemistry learning cycles (like BQeasy...)?
2)is there a way to set the under voltage protection value? I think now it is set on 2.5V, which is a bit (just a bit though) high.
3)in your experience, does the chip needs a cooling system, having transfering 1A sometimes through him for balancing?
4)in the application note I saw a thermistor for every cell, is it possible to connect only part of them? and if so, what should I connect instead?
thanks for any help
I'm very excited about this device!!