I have a customer asking about using Rrf values different from those shown in Table 1 in the DS.
The DS specifies 4 different resistances to achieve 4 different switching frequency "presets"
Would changing the Rrf to GND resistor to a value not in the table, change the switching frequency to a value not in the table?
IE, Table 1 says 470kΩ = Fsw of 290kHz, then 200kΩ = Fsw of 340kHz, etc...
Would a resistor value of 330kΩ for example, still have a Fsw of 290kHz, or 340kHz? or would it be different?
Also, page 4 of the DS shows for Fsw, that with a 470kΩ resistor, Fsw = 266kHz to 314kHz....But this was measured at 25℃...so is there that much discrepancy in the Fsw setting?
In short, could you clarify what the "preset" definition is, and what happens if a different resistor value is used that those listed in Table 1?
Thanks!
Darren