This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3492: Use this chip as Buck (Step-down)

Part Number: LM3492

Hi,

I want to use LED driver LM3492HC two drive to LED strings in my design.

The spec says that it is a boost, but I would like to use it as a step down (buck)

Example: 48V input with 35V output driving 200mA.

I asked Customer Support about this but they suggested to post my query in this forum instead.

Looking forward for some advice.

Thanks.

Regards,

Ryan