This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25882: Out of range when termination current at 50mA setting

Part Number: BQ25882

Hi,

It is written in the datasheet that an error when I set a termination current to 50mA is ±40%.
Therefore, the upper side is 70mA.
I measured termination current in two following environment.

1)    BQ25882EVM-001 + 2cell Battery + Ammeter (BAT+ <-Meter-> Battery)

2)    BQ25882EVM-001 + 2cell Battery + Voltage Meter (both end of R6(10mohm))

Even if several times of results measured termination current, it exceed 80mA.
Is this problem of device or EVM or setting?
In any event, please teach me the reason because I want to reappear.

Best Regards,
PAN-M