This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2813-4: Thresholds at 70V VCC

Part Number: UCC2813-4


Hello Team,

Good day! Need your inputs on this. Our customer wants to operate the UCC2813-4 at 70V and 60V VCC as the turn-on and off threshold respectively. Is it possible to do this through a voltage divider configuration at the supply stage? This is also while ensuring the given threshold value range and ICC at 30mA through the current limiting resistor. If so, are there any other conditions to be considered?

Thanks in advance!


Kind Regards,

Jejomar