This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Disable the AOLD protection function

Part Number: BQ40Z80

1. Customer wants to disable the AOLD protection function, is it possible ?
2. For AOLD and ASCD, only AOLDL and ASCDL (with L) are found in the Enabled Protections setting. Is it possible to set only the latch operation?

Best regards,
Kagawa

  • Hi Kagawa,

    1. The customer wants to disable the AOLD protection function, is it possible?

    [Andy]I don't think so. It is a hardware-based protection feature.


    2. For AOLD and ASCD, only AOLDL and ASCDL (with L) are found in the Enabled Protections setting. Is it possible to set only the latch operation

    [Andy] No. They are both hardware-based protection features.  

    Andy