Other Parts Discussed in Thread: TINA-TI,
Dear *,
on web page http://www.ti.com/product/CSD19534Q5A/toolssoftware there are two models PSpice and TINA-TI.
1) Can you tell are the both models the same but in different format or is the Pspice from 2020 better?
2) If they are not the same which one is new-er or better?
3) can both models bu used in TINA-TI
4) Can you tell also are booth models ok for using in AC and Transient simulation ?
5) Can you tell do booth model model the input capacitance Cgs and Cgd?
6) Can you tell do booth model model the input gate charge Qg Qgd Qgs?
Best Regards.