Hi, Team
There is following comment at description of pin function. Could you help to explain what does it mean? Thanks.
Input current limit of less than 500 mA is not support on ILIM pin.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Team
There is following comment at description of pin function. Could you help to explain what does it mean? Thanks.
Input current limit of less than 500 mA is not support on ILIM pin.
Hi Daniel,
The ILIM pin resistor sets a maximum input current limit clamp which supercedes the IINDPM register. In other words, the input current limit is the lower of the IINDPM register or the ILIM pin resistor setting. However, the ILIM pin resistor cannot be used to clamp the input current limit lower than 500mA. But the IINPDM register can be set to values below 500mA.
Regards,
Jeff