Hello,
I got 2 question on LM2674 :
-The current limit is a peak current, rms current or average current ? If the ripple current is big the protection current can actived ? For example Io= 500mA and ripple current =1Apk_pk at 12V?
- Have you a model for test the stability of the LM2674 ( on LTSPICE or other simulator free)?
Best regard,
William LIONI.