This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5852S-Q1: Boot Strap Power Supply

Part Number: ISO5852S-Q1

Hi, 

Is it possible to use bootstrap power supply for ISO5852S-Q1 ?? So that I shall require only three power supply for an inverter operation ??

Any specific disadvantages with the same??

Regards

Manoj R

  • Manoj,

    Thanks for your question.

    In fact, for an inverter design, you can even supply the lowside drivers from single isolated supply and use bootstrap on the highside.

    The advantage of bootstrap supply is reduced cost and complexity compared with transformer solution.

    The key disadvantage is that it cannot support keeping mosfets on for 100% of the time, as the bootstrap cap is replenished every off-cycle. If the off-cycle gets smaller and smaller, the bootstrap cap charge will not be able to be replenished fully. In this case, a seperate supply for high-side should be used.

    If you wish to have negative bias on your high-side using zener, the topology is different than if you used a seperate supply for high side and has limitations.

    Care must be used to properly select bootstrap capacitor, current limiting resistor, as well. The below report is an excellent reference on bootstrap circuit design.

    Alternative isolated supplies for high-side include push-pull, isolated flyback, etc. The advantage of using magnetic solutions, apart from allowing high duty cycle of the gate driver control, is that multiple rails can be generated via transformer in order to generate the negative bias supplies directly.

    We also have reference designs using isolated flyback as well as SN650x push-pull converter to generate isolated (highside) supplies. Compared with the aforementioned isolated flyback, this option has a smaller footprint.

    If this has answered your question, pleas let me know by clicking the green button. Otherwise, let me know if you have any additional questions.

    Best

    Dimitri

  • James,

    Thanks for the detailed explanation. 

    Is there any isolation limitation if we use single power supply for isolated top and bottom gate drivers ?

    Regards

    Manoj.R

  • Manoj,

    There shouldn't be any problem from the perspective of the drivers themselves. As long as the power strategy used can supply all the gate driver it itself should also be designed to meet the isolation required, such as transformer selection or similar.

    If this answered your question please let me know by clicking the green button. Otherwise, please let me know your further questions.

    Best

    Dimitri