Part Number: INA226
Just to clarify the datasheet, it says the shut voltage input range is -81.9175mV to 81.92mV ... that's differential, correct? And the absolute input range is still 0-36V on IN+ and IN- ? I'm a little bit nervous about using this on the high side. I'm trying to measure 0.8A to 1.2A at about 12 volts with a 0.1 ohm shunt resistor.