This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25118: LM25118: adjustable constant output current

Part Number: LM25118


Hi, I would like to use this or a similar suitable device to get an adjustable constant output current between 1A and 20 A out of 12V Vin. The current will be used in a chemical process. Could you give me some criteria or even a schematic diagram to get started.

thanks

  • Hi Felix,

    Thank you for reaching out.  You can put your load in series with a current sense resistor and feedback that signal such that the load current is regulated.  To reduce the losses, you need external Op-Amp to amplify the signal. Please refer to the attached block diagram of the concept.  Not all LM25118 pins are shown.

    CC Control-LM25118.pdf

    Thanks,

    Youhao Xi, Applications Engineering