Part Number: TPS84621
Hi all
I have TPS84621 and 12VDC Input voltage.
Therefor in need to put an resistor network in front of INH/UVLO input right?
In the datasheet, there is only up to 10V (Table 9)
What resistors do I need to select? (I assume it will not work when i use 8V VIN UVLO resistor settings?
There is also some reference schematic https://e2echina.ti.com/resized-image/__size/1230x0/__key/communityserver-discussions-components-files/24/dioe.jpg
but why is this GND connection to the left side of the capacitor??