Other Parts Discussed in Thread: CSD17579Q3A, BQ24773
I am already sucessfully using bq25703a with 12V input. I now want to change my design for 20V adapter input with max. 1.5A. Cell config is 4s (li-ion). I have a couple of questions:
- For my application I won't need the boost converter. Is it possible to omit boost converter FETs?
- Due to low current, I would like to use only one FET type. Is it possible to use CSD17579Q3A as buck FET and also as Battery FET?
- For my application with only buck, bq24773 would also be an option. However, it seems to be an "older version" of the bq25703a, are there any drawbacks?
Thanks in advance