This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340: Purpose of R5 and R6

Part Number: TPS55340


Hello.

At fig.16 on 9.2 Typical Applications, there are R5 (50 ohm) and R6 (0 ohm).

What is the purpose of these resistor ?

Do I need to add these resistor to my circuit ?

Best Regards.

  • Hi Shosuke,

    Thanks for your interest in TPS55340.

    R5 is for the loop measurement. It allows you to inject the perturbation at TP2 LOOP.

    R6 forms a RC filter for VIN in the case of high input noise and transient variation. However, the bypass cap C7 is usually enough, which is why R6 is 0. But it gives the flexibility to do RC filtering in case we need.

    Please let me know if you have other questions.

    Thanks,

    Yinsong

  • Dear Yinsong

    Thank you for your quick reply.

    I understand.

    Thanks and Best Regards.

    Shosuke