Other Parts Discussed in Thread: BQ25890,
Hi,
The first bits in REG09 hold temperature information. In the datasheet the different bit combinations are described as '000 – Normal,010 – Warm,011 – Cool,101 – Cold,110 – Hot'.
1. Which actual temperatures do these refer to. What is for instance 'Normal' and 'Warm'?
2. Can these bits be used to read the temperature of the IC at any time, or are they only updated if there is an actual fault?
3. If only updated when there is a fault, would there perhaps be a suggested way to trigger an intentional fault to get these temperature bits set?
Thanks!