This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM9061: Input and Output Capacitors

Part Number: LM9061
Other Parts Discussed in Thread: TPS2595, TPS25982, LM5060

Hi,

In the datasheet there is no much information on output capacitors. As for input side it is mentioned that he VCC pin must be bypassed with a capacitor with a value of at least ten times the Gate capacitance, and no less than 0.1 μF. In our design Vcc and Vout is 12V. Is it fine if only 0.1uF capacitor is bypassed from VCC and Cdelay=0.1uF for Delay pin is provided ?