This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5066I: Minimum slew rate when using dv/dt startup, is their a minimum and why?

Part Number: LM5066I

We are using the LM5066I configured with a dv/dt startup as per datasheet/application note. 

The datasheet itself does not specify a minimum slew rate and in fact states that the smaller the better. I have also had a searched online but did not find anything against small slew rate.

We are currently using 0.09V/ms giving us a startup time in the range of 580ms. (VinMax = 53V, Coutmax 2000uF). This appears to work correctly and we are getting the expected slew rate & startup time.

The confusion comes from the "LM5066I Design Tool- Rev. C" excel sheet which helps design this circuit. This document DOES  implement a minimum slew rate of 0.12V/ms.

The worksheet sheet used for calculation implements the limit in the following cells with hardcoded values: (Note, this is in a locked, hidden sheet titled dv_dt_recommendations)

Upper bound Slew Rate (4ms start-up) (V/ms) 12
Min Slew Rate (400 ms start - up) (V/ms) 0.12

Question 1: Is the minimum slew rate implemented in the excel workbook an arbitrary low value to allow this workbook to work correctly or is their an underlying IC limitation?

Question 2: The document refers to a 400ms startup, but the datasheet does not mention a maximum startup time, is their an IC limitation?

 

Regards,

Alexis

  • Hi Alexis,

    There is no limitation on the minimum slew rate. It was defined in the design sheet based on our past experience as we would be able to start large capacitive loads with 0.12V/ms slew-rate.

    Please unlock the tool with password LM5066I and modify to set lower slew rates.

    Best Regards, Rakesh