Part Number: TPS7A7100
Hi,
Customers use TPS7A7100 under the following conditions:
・Vin=3.3V, Vout=3V, Iout≒300mA
・Cin:0.1uF, Cout=10uF, 1uF, 0.1uF (ceramic cap), Cff=0.1uF
In the above situation,
Output oscillation occurred which is thought to be caused by the input side.
Customers are trying to improve on the following in their data sheet:
I got three questions from a customer about datasheet ”About Input Capacitor Requirements”.
1.Could you tell me the mechanism or principle of TPS7A7100 oscillation in the following cases?
"For example, a 5-nH inductor and a 10-µF input capacitor form an LC filter that has a resonance at 712 kHz.
This value of 712 kHz is well inside the bandwidth of the TPS7A7100 control loop."
2.Please tell me the target of resonance frequency by C and L.
Customers want to know the resonance frequency that should not be exceeded.
3.The typical characteristics were acquired under the condition of Cin = 10uF.
In this case, what is the assumed inductance due to the PCB, etc.?
Could you give me your advice?
Regards,
Yusuke