Part Number: BQ27750
I have two questions related to the following portion of a circuit in development that uses the bq27750. It is used in an embedded application, such as how a smart phone would have a permanent battery, rather than in a cordless drill with interchangeable self-gauging packs.
1) As hooked up, it looks like SRN and SRP are reversed, and SRN should be the more-negative voltage. This was observed in review sessions, but unwinding the "designed to be in a pack" schematic in the datasheet and EVM gives us a shred of doubt that reversing the connections so SRN is more-negative is actually correct. Please help us confirm the correct orientation.
2) Our charger IC has been assigned control and biasing of the thermistor in the pack as it can more directly control battery safety by charging only at appropriate temperatures. That leaves the bq27750 without a pack temperature to use for impedance tracking. Is it possible to use the bq27750's internal temperature sensor as the sole temperature input for IT, trusting that it will be close-enough to pack temperature? Do I just disable TS1 and enable Internal TS in the "Temperature Enable" register and then Impedance Tracking uses the inputs it has available? The other option is to add a board-mounted thermistor just for the bq27750, but we are hoping to avoid that.
Thank you.