Part Number: BQ25713
Hi team,
A customer of mine is looking to develop a product which would have 3 Li-Ion battery cells (3,7V 18650 batteries).
The BMS is just a small part of their design, so they are in search of a complete battery charging (BMS) solution which requires minimal design efforts.
In other words, a complete system to charge the battery and power the system with little or no external components required.
They looked at the BQ25713, but this device requires other components to be operational.
Some key careabouts:
Cell balancer required
USB-C communication path with adapter
Also interested an answer or application example that shows the combination for example between USB-C PD and the BQ25713 (How the fet switch is controlled).
I checked our portfolio and I could find a solution thats meet the above specs.
Can you help out with this request?
Thanks a lot for the support.
Obinna.