Part Number: TPS546A24A
I am trying to understand how to properly do pin strapping for TPS546A24A. One confusion is what is regarding initial contents of EEPROM. I think the default values for the EEPROM are in table 6. Is this correct? I am trying to figure out how to get the correct VSEL pin strapping. The requirements I have is that the voltage is adjustable between 0.8 and 0.94V with 10mV step size. Based on table 12 and the excel pinstrap calculator this does not seem possible but then table 13 seems like it should be possible. Can you explain what the two tables are trying to convey? Thanks