This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3843A: Needed Outpu of 15V, 1A

Part Number: UC3843A
Other Parts Discussed in Thread: UC2842, UC3843

Hello Guys,

Using the schematic from Figure 25 of the datasheet below, if the customer will replaced UC2842 with UC3843, can he achieved an output of 15V, 1A ? If so what modifications might he needed to do?

Thanks in advance!

Art

  • Hi Art,

    Sorry for the delay response due to the holiday.

    UC3843 can be used to replace UC2842, they have same maximum duty cycle, but please note that they have different UVLO thresholds and different acceptable ambient temperature range.

    And I suggest to redesign the schematic because of different output voltage and power, especially transformer, RFBU/RFBB and MOSFET. 
    Regards,

    Teng

  • Hi Teng,

    No worries about that and thank you very much. I will relay the information to the customer and will inform you for any additional inquiries.

    Thanks!

    Art