Is there any recommendations to tie the +15 and -15V lines together to acquire a ~ +30V output from this module? If so, please advise.
Input Voltage: Nominal 24V (18-36)
Output Voltage Required: ~30V
Output Power: ~1W
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any recommendations to tie the +15 and -15V lines together to acquire a ~ +30V output from this module? If so, please advise.
Input Voltage: Nominal 24V (18-36)
Output Voltage Required: ~30V
Output Power: ~1W
Thank you.
Hi Neel,
When connecting the outputs of a dual-output DCP02 in series, I would recommend the following schematic (Figure 36) in the datasheet.
Regards,
Alejandro