Other Parts Discussed in Thread: ADS1278-SP, , TL1431-SP, ADS1278, LMP2012, TINA-TI, DS90C031, SN55LVDS31
Hi, I want to use LM4050QML-SP (+2.5V) as voltage reference for the ADC ADS1278-SP. Input voltage is +5V and the ADC modulator frequency is 128 kHz (clock is 512 kHz). What external series resistor value is required between the input voltage and the LM4050QML? How stable is the output since the ADC is dynamic load? Can I get 16-bit resolution with the combination?
Thanks in advance
Dinakar