Iam doing a project which need to charge li ion battery from solar cell which will provide 7V, 70mA at peak time.I am using 3.7V , 1000 mAh battery and also I don't need to fully charge my battery through solar cell at least 60% charging is sufficient.
Because my application just need 120 mAh load current for 4 hr.
1000×60%= 600mah
600mAh/6hr= 100mah
100*3.7/5.6=66mA
So pls help me to find a better device