This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Single li io battery charging from less power solar cell

Other Parts Discussed in Thread: BQ24210

I need to charge li ion battery from solar cell and it's output like be 7V,70mA

Iqm using 3.7V , 1000 mAh battery and also I don't need to fully charge my battery through solar cell at least 60% charging is sufficient.

Because my application just need 120 mAh load current for 4 hr.

1000×60%= 600mah

600mAh/6hr= 100mah

100*3.7/5.6=66mA

So pls help me to find a better device