From power up (VDD applied) when is SMBus interface become available to accept master access?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
From power up (VDD applied) when is SMBus interface become available to accept master access?
Thanks. As for pullups on the SCL/SDA/SMALERT, because the internal 3.3V regulator capacity is limited, I plan to use external voltage to supply the pullup If the external 3.3V is applied to the pullup before 12V is applied to TPS40422, do you see any issue messing up the internal state machine?
Hello,
It is fine that external 3.3V voltage (pull-up voltage for SCL/SDA/SMALERT) comes before 12Vin.
Thanks
Qian
One last question: I'm not sure how exactly ADDR[1:0] work.
According to the datasheet, ADDR1 sets the 10s digit while ADDR0 sets the 1s digit. For example, if 127K pull down is on ADDR1, and 38.3K pull down on ADDR0, the I2C slave address would be 63. Is it correct? Is 63 a decimal or hex? Is it 7-bit address or 8-bit addrss?
Then if you look at the reference design in the datasheet both ADDR1 and ADDR0 are pulled down by 36.5K ohm, which isn't defined by Table 3 on page 26. So what 8-bit hex address does it strap the device to?
For reference, the 8-bit address means to pad 0 at bit[0]. You know bit[0] is read/write indicator in the I2C protocol. A 7-bit address 7'b1010000 would be equivalent to 8-bit address 8'b10100000.
Thanks..
The 7 bit address consist of 0b+ADDR1+ADDR0. Both ADDR1 and ADDR0 are 3bits.
For example, if resistor is 38.3k, it means 011b. If resistor is 82.5k, it means 101b.
The 8 bit address is 7bit address followed by r/w bit.
The EVM was released by others many years ago, I have no idea why 36.5k is used. Please refer to datasheet table 3 to select resistor value.
Thanks
Qian