This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ29209: using the part as balancing only

Part Number: BQ29209


I'm planning to use the bq2920x to balance a 2 cell battery, I do not care for the protection circuit. Can I leave the RVD, CVD, CCD out and connect the VDD directly to PACK+? Will the balancing functionality be affected? I'm space limited.

  • Hi Dusan,

    From a safety perspective, we cannot recommend removing these components. The removal of CCD will cause the over-voltage detection delay to move toward zero. RVD is needed for battery safety in the case there is a hard short from VDD to VSS internal to the device. It is not a requirement for proper device operation, but the device functionality has not been characterized without these components.

    Best regards,

    Matt