Other Parts Discussed in Thread: TPS62140
Hi,
I have a battery powered application using a sealed lead acid battery. I need a 3.3V power converter for the battery output, so the input range needs to include potentially a 8V float voltage. I need 2 amp output when the board is in active mode. In sleep mode I of course would like to have the lowest possible current draw. The TPS54321D fulfills most of these requirements, but I would wish for a lower operating current while in sleep mode than the 75uA draw by the TPS54321D. Is there a solution with less operating current? I have a load in sleep mode less than 60nA. If a suitable power converter does not exist, I am toying with the idea of having 2 3.3V converters, one for sleep mode and one for active mode. I would disable the TPS54231 in sleep mode. This requires a converter with lower output current, maybe 10mA or there abouts and of course a very low operating current. The 2 outputs would be OR'd together with a FET based OR'ing device.
Any help with these requirements will be appreciated. I have tried parametric solutions but am never sure that I have not inadvertently eliminated viable options.
Thanks, Phil