Other Parts Discussed in Thread: BQ25896, BQ25601, BQ24298
Hi
I planning to use the bq24259 charger in a design. When the product are used it will only be powered by the battery. When turned off the supply to all internal electronics shall be turned off. I plan to use the shipping mode for that and let the micro-controller turn of BATFET thru the I2C bus. There is a push-button that are used for power on/off and other HMI tasks. A short press shall turn it on and a long press turn it off. The button will connect both to QON pin and to our micro-controller.
Is the turn on detection on QON based on rising flank or level?
What happen when BATFET turns off thru I2C bus and QON is still high level due to our long press turn off action?
Will BATFET turn off when I2C write command is complete after stop command or before?
When BATFET turns off, the supply to the micro-controller is lost. Is there any risk to leave the I2C bus on bq24259 in a locked state when this happens?
When are power on reset performed? If battery voltage are always present, is there any power on reset when the charger is connected?
Best regards
Magnus