Other Parts Discussed in Thread: TPS563210A
Hi,
I have two questions related to each other:
1) is it possible that the TPS65381A-Q1 has a value less than 3.24V as the value of VDD3 / 5 (set to have 3.3V)?
For example, can this value be 1V?
2) And if so, being connected to the EN pin of the TPS563210ADDFR component,
would it belong to the indeterminate band between VENL and VENH, how does the TPS563210A behave?
Thanks.