WE HAVE A DESIGN WITH +5V VIN TO GENERATE +/- 3.5V OUTPUT. THE DESIGN HAS BEEN IMPLEMENTED ON WEBTOOLS TO THE LETTER. THE PROBLEM WE ARE SEEING IS THE -VE O/P IS FLUCTUATING BADLY BETWEEN -2V TO APPROX -4.5V THAT LOOKS LIKE A SAWTOOTH WAVEFORM. ALL CONNECTIONS AND COMPONENTS HAVE BEEN CHECKED AND REPLACED. THERE IS APPROX 50mA DRAIN ON +VE O/P AND ONLY 2mA ON THE -VE O/P. i HAVE ADDED EXTRA LOAD TO BALANCE THE -VE BUT PROBLEM STILL EXISTS, THE FREQUENCY OF THE SAWTOOTH JUST INCREASES SLIGHTLY. THIS IS A 3RD PARTY DESIGN SO I CAN'T SUBMIT SCHEMATICS. ANY HELP WOULD BE APPRECIATED.