Hi!
my customer uses this device and notices, that the CPU often times access the BIT DECAY (BIT0) and sets and deletes it.
Why is that?
And what is this register for?
Kind regards,
Marion
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
my customer uses this device and notices, that the CPU often times access the BIT DECAY (BIT0) and sets and deletes it.
Why is that?
And what is this register for?
Kind regards,
Marion
Marion,
I'm sorry, but I don't see "BIT DECAY" or "DECAY_BIT" or any meaningful combination of these 2 words anywhere in the TPS65094 datasheet.
Can you be more specific about the register you are referring to? Do you know what the I2C Address is? Are you using an I2C Analyzer (like the Saleae or TotalPhase Beagle) that will allow you to print a datalog?
It is possible the naming conventions used by Intel are different than those in the TI datasheet, but I do not have any way to map the Intel CPU command to the PMIC Registers.
Marion,
I have learned that this bit is a bit in the BUCK1CTRL register (address 20h).
This is a RESERVED bit, but its original name was BUCK1_ DECAY and it is a R/W bit. The definition is as follows:
Decay Bit
0: The output slews down to a lower voltage set by the VID bits.
1: The output decays down to a lower voltage set by the VID bits. Decay rate depends on total capacitance and load present at the output.
Since this bit is RESERVED, we advise that you do not modify any code which accesses this bit. However, it is not an issue if Intel code is modifying this bit. Intel was informed of the original name and definition of this bit.