Other Parts Discussed in Thread: BQSTUDIO
Hi Ti Experts,
we want to use the bq76952 in standalone mode for a 16S6P (21,6Ah) LiFePo application.
So far we have designed and produced a first PCB version.
If I calibrate the current gain with the bqStudio function the "CC Gain" and the "Capacity Gain"
in the Data Memory are changing to good values, I think:
We are using six 3mOhm Shunts in parrallel. So the value is ok.
Now I have exported the whole DataMemory in a *.gg.csv file.
If I reset the bq or use a new one I want to import the saved *.gg.csv.
I am using the "Import from File (Advanced) function":
I am selecting all values:
After that I push the "Write_All" Button:
And than I get this message:
Is this an error of the bqStudio? Does the program not allow the change?
Thanks for helping us.
Klaus