This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53681: TPS53681 NVM save times and VOUT_COMMAND to VBOOT

Part Number: TPS53681

Hi:

 How many times can TPS53681 NVM save user configuration?

TPS53681 controller whether different voltage settings are supported for VBOOT and VOUT_COMMAND,for example VOUT_COMMAND=0.80V,VBOOT=0.86V?

If this application is supported, how can VBOOT=0.86 voltage jump to VOUT_COMMAND=0.80V voltage?

thanks

  • Hi,

    1. TPS53681 can support at least 1000 times NVM written.

    2. After TPS53681 initialization (3.3V is ready), VOUT_COMMAND will be the same as VBOOT. Then after device boot up to VBOOT, you can send out the desired voltage to VOUT_COMMAND to change VOUT.

    Thanks