Tool/software: WEBENCH® Design Tools
sir, design has been referred from webbench and model with .tsm format has been used from TI even then output is not appropriate .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
sir, design has been referred from webbench and model with .tsm format has been used from TI even then output is not appropriate .
sir,
this is the web link for case generated with same issue with the help of your customer support channel.
in this circuit has been shared which was simulated in tina software referred for your webbench design .
thanks
Hi, SAJAL
The link cannot be open.
Could you send me the PDF or screenshot file?
Hi, SAJAL
1. I review the schematic, just one comment:
Disconnect R64, and connect a resistor between Rosc pin and GND, which is set operating frequency, you can refer Page10 of datasheet.
2. Could you send me your modified TINA model? I want to do the simulation.
Hi, SAJAL
I can run your modified model, Vout1, Vout2 and Vout3 were set to same value(1.5V).
I have changed the divider resistors, and we can get Vout1=1.5V, Vout2=1.35V, Vout3=3.3V.