This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5033: Unstable operation of Duty

Part Number: LM5033

Hi Team,

My customer evaluates it using the LM5033MM.

The external sync is working, but the duty is not close to 50%.

ON OFF Duty is 30% -70% operation, which is unstable operation which is 70% -30%.

If it is operated without a sync signal, it will operate at a Duty of nearly 50%.

Why is the operation unstable when a sync signal is input?

The surrounding conditions are as follows.

 Rt / sync: 36kΩ-GND / 100pF-Sync (90kHz, 3.8V)
 SS: 5V
 COMP: Open
 Ref: 0.1uF-GND

I also got the schematic from the customer and would like to send it in a private message.

Best Regards,

Kenji