This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM66100: What happens between Von and Voff?

Part Number: LM66100

Hello,

There is an undefined region between the Von and Voff conditions for Vce - Vin.  Specifically, when Vce - Vin is between -80 mV and 0 V, the operation is not clear to me.  Is there inherent hysteresis such that the direction of the voltage change defines the state, so that if the device is on and trending toward off, it stays on through that region, but if it is off and trending toward on, it stays off through that region?

Thanks,

Scott