Hello,
In section 7.3.4 of the datasheet, it states "The current limit threshold, VCSMAX, defines the voltage on CS above which the GATE ON time will be terminated regardless of the voltage on CTL." However, looking at the Functional Block Diagram of section 7.2, it appears that having a signal on the CS pin which exceeds VCSMAX (~0.55V) would set the internal flip-flop's CLRB low which then sets the GATE output high, regardless of the voltage on CTL. Can you clarify which is correct?
Thanks,
Michael