This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542-G1: BQ27542-G1 learning cycle

Part Number: BQ27542-G1

Hi there, is it necessary to set "Load Mode" and "Load Select" during a learning cycle? Will this  parameter effect leaning accuracy? thanks.

I copy the below paragraph from TRF, is that means system recalculate power no matter  how "Load Mode" and "Load Select"  before

For simulations during RELAXATION, CHARGE, and at the start of DISCHARGE (since a new average
has not been gathered), it would use data flash values for simulations. Once the discharge lasts 500
seconds, the gauge re-simulates using the new running average. Thereafter, during discharge, it uses the
continuous running average for any subsequent simulations. Re-simulations can also be triggered by a
temperature change, which can cause an updated simulation to occur earlier than 500 seconds into a
discharge. In this case, this simulation would use the present running average.

 

B.R

Mike