This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: BQ25895

Part Number: BQ25895

Hi

I am using BQ25895 IC. I want two type A USB ports at the output that will power my two usb devices.

This module is having one PMID output and it outputs 5 volts and 3 Ampere

My questions are:

1. How to draw two A type USB ports from single PMID output

2. What i need to do if i want one USB port output current is 2 ampere and other USB port output current is 1 ampere